About memory map in S32K3XX.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About memory map in S32K3XX.

2,760 次查看
Changhawn
Contributor IV

In S32K3 MCU, Our project use the FreeRTOS, lwip, mbedtls (w HSE), and other user protocols. But Int_sram section overflowed by 180k,
so Memory map for loader(Linker) is defined like below.
Is it ok for working? or Can you provide a recommended memory map?


MEMORY
{
int_pflash : ORIGIN = 0x00400000, LENGTH = 0x003D4000 /* 4096KB - 176KB (sBAF + HSE)*/
int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */
int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00010000 /* 64KB */
int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0001F000 /* 124KB */
int_stack_dtcm : ORIGIN = 0x2001F000, LENGTH = 0x00001000 /* 4KB */
int_sram : ORIGIN = 0x20400000, LENGTH = 0x0005D800 /* 184KB + 182KB(For user application), needs to include int_sram_fls_rsv */
int_sram_fls_rsv : ORIGIN = 0x2045D800, LENGTH = 0x00000100
int_sram_no_cacheable : ORIGIN = 0x2045D900, LENGTH = 0x0000FF00 /* 64KB, needs to include int_sram_results */
int_sram_results : ORIGIN = 0x2046D800, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x2046D900, LENGTH = 0x00004000 /* 16KB */
ram_rsvd2 : ORIGIN = 0x20471900, LENGTH = 0 /* End of SRAM */
}

0 项奖励
回复
5 回复数

2,741 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Changhawn

You didn't mention the part number you're using.

This is can be done,  but you need to consider that this part of the content was originally reserved for flash driver related functions(etc, C40_Ip). If you need to map function to this area, then you need to think it twice.

0 项奖励
回复

2,737 次查看
Changhawn
Contributor IV

Hi Senlent.

Developing with sample project is for S32K344 and S32K344 Eval board.

We also have to use flash driver. Could you tell more in detail about added reserved area? or suggest other memory map solution? 

Thank u.

Chang

0 项奖励
回复

2,721 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Changhawn

Could you tell more in detail about added reserved area?

Looking at your linker file, you have used all the SRAM. 

 

0 项奖励
回复

2,718 次查看
Changhawn
Contributor IV

Hi Senlent.

I meaned that "reserved for flash driver related functions(etc, C40_Ip)". 

I can not find any clue about this in linker file.

Thank u.

Chang.

0 项奖励
回复

2,674 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Changhawn

in the linker file you can find the below sentence:

.acfls_code_ram :
{
acfls_code_ram_start = .;
*(.acfls_code_ram)
acfls_code_ram_stop = .;
} > int_sram_fls_rsv

 

you can add c40_ip related api to this area:

"__attribute__((section (".acfls_code_ram"))) xxfunction(or xx variable)" 

0 项奖励
回复