About FLEXIO Timer Operation Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About FLEXIO Timer Operation Question

1,906件の閲覧回数
584914019
Contributor III

52.4.3.6 Timer Disable and Stop Bit

Timer output will clear. Shifters that are controlled by this timer do not see this as a
falling edge on the timer shift clock, but can generate a shift event if the timer shift
clock would otherwise generate one

This description is incomprehensible, can you elaborate on it

0 件の賞賛
返信
3 返答(返信)

1,829件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

To provide you better support, could you please specify where exactly did you see that description? 

Regards, 

Victor 

0 件の賞賛
返信

1,829件の閲覧回数
584914019
Contributor III


S32K-RM-2019 52.4.3.6 chapter

0 件の賞賛
返信

1,829件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

You have an old version of the S32K reference manual, you can download the newest version available from the following link.

Now regarding the statement. When the condition configured by timer disable (TIMDIS) is detected, the output of the timer will be cleared, it doesn't matter what is the value of the timer, once this condition is detected this output will be cleared automatically. Clearing the output of the timer won't affect the shifters controlled by this timer, this means that the values won't be shifted when this condition occurs unless you generate a shift event with the timer shift clock. 

Regards, 

Victor 

0 件の賞賛
返信