AUTOSAR OS S32K1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,509件の閲覧回数
liuruowen
Contributor I

Hello:

I used S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0 and got a problem, as shown below:

liuruowen_0-1600398059935.png

cannot generate the above files,what's the reason?

compiler:gccarm   Ver:4.9.3   Path:C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v4.9\gcc-arm-none-eabi-4_9

GUN Make Ver:3.81

liuruowen_1-1600398339386.png

 

0 件の賞賛
返信
1 解決策
2,495件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPG

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,496件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPG

Nam

0 件の賞賛
返信