AUTOSAR OS S32K1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR OS S32K1

Jump to solution
2,489 Views
liuruowen
Contributor I

Hello:

I used S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0 and got a problem, as shown below:

liuruowen_0-1600398059935.pngliuruowen_0-1600398059935.png

cannot generate the above files,what's the reason?

compiler:gccarm   Ver:4.9.3   Path:C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v4.9\gcc-arm-none-eabi-4_9

GUN Make Ver:3.81

liuruowen_1-1600398339386.pngliuruowen_1-1600398339386.png

 

0 Kudos
Reply
1 Solution
2,475 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPGPath_Java.JPG

Nam

View solution in original post

0 Kudos
Reply
1 Reply
2,476 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPGPath_Java.JPG

Nam

0 Kudos
Reply