AUTOSAR 4.4 MCAL Port Module configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR 4.4 MCAL Port Module configuration

2,960 Views
jwjung
Contributor II

hi, 

 

i have some question about using MCAL Port Module.

 

jwjung_0-1753244978665.png

in configuration, PortPin Slew Rate be set 0 but in generated code that parts are empty so that build error occured.(and i can't change that)

jwjung_1-1753245109044.png

 

second, 

i enable the Api to change PinMode and PinDirection, but can't call that function.

jwjung_2-1753245304099.pngjwjung_3-1753245385753.png

The gpio output control could not be performed because the direction of the port pin could not be changed.

 

give me some advise to use the MCAL Port Module.

thank you.

 

0 Kudos
Reply
7 Replies

2,950 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jwjung

Could you please tell me the RTD version you're using?

Also could you please open a example related to port in S32 DS and test again?

0 Kudos
Reply

2,944 Views
jwjung
Contributor II

hi,

 

i used RTD 2.0.2 version.

i tried to use example pjt but i can't solve the problem like below.

 

jwjung_1-1753260614440.png

 

thank you

0 Kudos
Reply

2,941 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jwjung

This should not be an error. You need to select the pins first in the "Pins" configuration interface.

Senlent_0-1753265563780.png

 

0 Kudos
Reply

2,921 Views
jwjung
Contributor II

hi,

 

in my mistake, transmitted other data.

 

i used SW32K3_RTD4.4_R21-11_3.0.0_D2303 

and i wanna know about 

 

jwjung_1-1753349619423.png

in example code the configuration data is differ from mine.

example is not PortPin_Mode is __IN, it's GPIO, AND PortPin Slew RAte, PortPin Level Value is differ from mine.

 

can you advise me to do it right?

 

thank you.

0 Kudos
Reply

2,900 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jwjung

Please let me know which pin you want to configure? I can configure it and take a screenshot for your reference.

0 Kudos
Reply

2,894 Views
jwjung
Contributor II

hi

 

i'm trying to use PTB8 for GPIO port pin. and i named it LED1. 

so that i configure the value like this.

jwjung_0-1753409327660.png

picture 1) Port Configuration - PortConfigSet - PortContainer_0

 

jwjung_6-1753410044759.png

picture 2) Port Configuration - PortGeneral

 

jwjung_1-1753409339892.png

picutre 3) Dio Configuration - DioConfig 

 

jwjung_3-1753409464470.png

and the PIN_PORT BE generated like this. so that i write the code like below.

 

jwjung_4-1753409527815.png

so, my question is, 

i configure the configuration to use SetPinDirection and setPinMode Api but i can't call the function to use.

 

and the Port parameter is differ and do not initialize.

jwjung_5-1753409786627.png

 

how do i have to do solve this error.

 

0 Kudos
Reply

2,888 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jwjung

RTD 2.0.X is already a very old version. The latest RTD version has been updated to RTD 6.0.0. And S32 DS V3.4 is also a very old IDE.
My suggestion is to install S32 DS V3.6 and RTD 6.0.0.

If you still encounter these problems on the new version, I can make some demos for you for reference.

0 Kudos
Reply