AN12218SW Bootloader doesn't properly reset SCG->FIRCDIV and PCC->LPUART prior to app jump.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AN12218SW Bootloader doesn't properly reset SCG->FIRCDIV and PCC->LPUART prior to app jump.

跳至解决方案
1,391 次查看
lucianomoretti
Contributor IV

While debugging peripheral clocking issues after jumping from the bootloader I found the following in the clocks.c reset_clock() function:

SCG->FIRCDIV |= SCG_FIRCDIV_FIRCDIV2(0b000); /* Disable FIRC divider */


This code does not change the FIRDIV register because it is an "or" with zeros.

The corrected code is:

SCG->FIRCDIV &= ~SCG_FIRCDIV_FIRCDIV2(0b111); /* Disable FIRC divider */

 

The code also does not restore the clock source for the LPUARTs in the Uart.c void UART_Reset(LPUART_Type *pUART) function to the original clock source of '0', leaving it set to clock source 3 as set in the UART_Init function.

0 项奖励
回复
1 解答
1,383 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

thank you for bringing this into our attention, I will report it. The application note should be updated in the near future.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,384 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

thank you for bringing this into our attention, I will report it. The application note should be updated in the near future.

Regards,

Lukas

0 项奖励
回复