ADC project using MCAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC project using MCAL

7,627件の閲覧回数
laofu
Contributor II

HI,@NXP

I try to build a ADC project triggered by pdb using s32ds with autosar mcal,whether just the mcal module ADC is needed,should the drivers module Adc_Ip and pdb_Adc_Ip is needed? thanks

laofu_0-1678906669186.png

 

0 件の賞賛
返信
7 返答(返信)

7,592件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
If you added Adc in MCAL module, don't need to add PDB_Adc_Ip under Driver layer

0 件の賞賛
返信

7,577件の閲覧回数
laofu
Contributor II

thinks for your replying,I want the pdb trigger by Lpit ,but in mcal ADC module,i can not configure the pdb to trigger by hardware,it seems that pdb  can only triggered by software.My ultimate aim is just using mcal to configure a project that adc is triggered by pdb ,and pdb is triggered by Lpit.

 

0 件の賞賛
返信

7,453件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Sorry for late response,
I created the example ADC trigger by LPIT in the attached file and the guidance to configure and implement for example. please look at these attachments

0 件の賞賛
返信

7,436件の閲覧回数
laofu
Contributor II

HI,thanks.does the example project you provided is mistake? it seems about i2c.  in addition,my RTD is 1.01and this example use RTD1.0.0, so i can not open it

0 件の賞賛
返信

7,425件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Sorry, I make mistake when upload the example
I re-attached the ADC project for K1 RTD 1.0.1

0 件の賞賛
返信

7,556件の閲覧回数
cuongnguyenphu
NXP Employee
NXP Employee

Can you give me the information of hardware target and RTD version you're using?

0 件の賞賛
返信

7,548件の閲覧回数
laofu
Contributor II

Hi,

i use the s32k144,and RDT version is 1.0.1.

0 件の賞賛
返信