ADC failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,952件の閲覧回数
LinWeiyang
Contributor II

I tested the ADC pins using the S32K312 chip and found that the IO pin PTE18 did not successfully convert data, but the other two pins, PTC7 and PTD28, both worked successfully as ADCs. In the IDE, the configurations for these pins are almost identical. Observing the schematic diagram, I did not find any pull-down situation for the PTE18 pinPTC7.pngPTD28.pngPTE18.pngcode.pngconfig.pngconfigPTE18(2).pngconfigPTE18.png

タグ(2)
0 件の賞賛
返信
1 解決策
1,886件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try to call Siul2_Port_Ip_Init and check it again.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,920件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please tell me what version of RTD you are using.
Please check bit 6 MUX_MODE_EN_ADC1_S23 of 38.2.51 Read Write GPR On Functional Reset 4 (DCMRWF4).


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,893件の閲覧回数
LinWeiyang
Contributor II

Is here wrong ?

 

1.png2.png3.png

タグ(1)
0 件の賞賛
返信
1,887件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try to call Siul2_Port_Ip_Init and check it again.

0 件の賞賛
返信
1,914件の閲覧回数
LinWeiyang
Contributor II

I used SW32K3_RTD_R21-11_4.0.0_P04_D2312 as my RTD.However,I changed it to SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410,the result is same.0x402A.pngMemory.pngzip.png

タグ(1)
0 件の賞賛
返信