ADC failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ADC failed

跳至解决方案
1,863 次查看
LinWeiyang
Contributor II

I tested the ADC pins using the S32K312 chip and found that the IO pin PTE18 did not successfully convert data, but the other two pins, PTC7 and PTD28, both worked successfully as ADCs. In the IDE, the configurations for these pins are almost identical. Observing the schematic diagram, I did not find any pull-down situation for the PTE18 pinPTC7.pngPTD28.pngPTE18.pngcode.pngconfig.pngconfigPTE18(2).pngconfigPTE18.png

标记 (2)
0 项奖励
回复
1 解答
1,797 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try to call Siul2_Port_Ip_Init and check it again.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,831 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please tell me what version of RTD you are using.
Please check bit 6 MUX_MODE_EN_ADC1_S23 of 38.2.51 Read Write GPR On Functional Reset 4 (DCMRWF4).


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,804 次查看
LinWeiyang
Contributor II

Is here wrong ?

 

1.png2.png3.png

标记 (1)
0 项奖励
回复
1,798 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please try to call Siul2_Port_Ip_Init and check it again.

0 项奖励
回复
1,825 次查看
LinWeiyang
Contributor II

I used SW32K3_RTD_R21-11_4.0.0_P04_D2312 as my RTD.However,I changed it to SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410,the result is same.0x402A.pngMemory.pngzip.png

标记 (1)
0 项奖励
回复