ADC_DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC_DMA

2,265 次查看
Ayaz
Contributor IV

I am using the S32K344 with RTD version 5. I have designed my ADC signal readings to be read in a specific sequence, offset by eMIOS triggers. Currently, I am reading the ADC data using Bctu_Ip_GetFifoData(). The system works as expected, with BCTU_IRQn interrupts for FIFO1 and FIFO2.

Now, I need to switch to DMA, using DMATCD1_IRQn for FIFO1 and DMATCD16_IRQn for FIFO2. The issue I am encountering is that I am unable to read the signals for FIFO2 unless I disable the interrupt for FIFO1, and vice versa. I have attached my project so you can have a closer look at the issue.

标记 (1)
0 项奖励
回复
6 回复数

2,148 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

Please find attached project.

This example implements two BCTU lists for parallel conversions using ADC0 and ADC1. Each conversion is triggered by a separate PIT channel, and the resulting data is stored in FIFO1 and FIFO2, respectively, as follows:

PIT ch0 -> BCTU List 1 -> FIFO1
ADC0: S10 and VREFL
ADC1: Bandgap and VREFH

PIT ch1 -> BCTU List 2 -> FIFO2
ADC0: VREFH and Bandgap
ADC1: VREFL and S10

_Leo__0-1750201623389.png

Note that ADC channels are used by both ADC instance in both BCTU lists. So S10 with ADC0 is routed to PTD3, meanwhile with ADC1 is routed to on-board potentiometer.

Please use S32DS 3.6, RTD 5.0.0 and S32K3X4EVB-T172.

I hope this information is helpful.

0 项奖励
回复

2,131 次查看
Ayaz
Contributor IV

Hi,

Thanks for your response. Based on my previous description, I want to use DMA with a custom design NOT BCTU:

The design I am building is to read ADC data from FIFO1 register using DMA Channel 1 and read ADC data from FIFO2 register using DMA Channel 16, storing both in one software buffer.

  • FIFO1 register --> software buffer[21]
  • FIFO2 register --> same software buffer, but needs an offset value of the signal number of FIFO1 signals .The Total ADC signals are 21.

Here the main issue:

I have chained Channel 1 and Channel 2, so when Channel 1 completes its major loop, Channel 2 should start transferring the data.

Channel 2 configurations:

  • Source: software buffer[21]
  • Destination: software buffer[210]

But the system is not working. I have attached my project so you can easily identify the issue. I would appreciate it if you could have a look and find the reason for the issue.
in adddtion to that i aslo have an issue :
Since the destination address [21] for both Channel 1 and Channel 16 is the same, Channel 1 reads 16 signals from FIFO1 and Channel 16 reads 5 signals from FIFO2, totaling 21 signals. How can I offset the destination address for Channel 16 by 16 in the DMA configurations? Currently, I am using a software offset, but I would like to do it in the DMA configurations.

Skærmbillede 2025-06-18 144433.png

标记 (1)
0 项奖励
回复

2,088 次查看
Ayaz
Contributor IV

I have not received an answer yet

0 项奖励
回复

2,061 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Ayaz,

seems you had just wrong DMA config, did not enable channel linking and had incorrect Transfer control for DMA channels. See attached modification I did...
Buffers are then filled, not sure if properly as you set system to transfer just raw data

PetrS_0-1750420165391.png

Hope it helps.

BR, Petr

 

0 项奖励
回复

2,034 次查看
Ayaz
Contributor IV

Thanks for your response. It works now.

Now, I have a question regarding the configuration of CH2. The source buffer is an array of 21 signals, but I only want to transfer the first 16 signals into the destination buffer. There will be 10 samples in total, making 160 samples. The destination buffer is of size 160 and uses the unsigned16 data type.

However, in the CH2 configuration, it is possible to transfer 32 bytes at a time, which is my full data per minor loop. So, I have changed my configurations to:

  • Source transfer size: 32 bytes
  • Destination transfer size: 32 bytes

But it is not working. Do you know the reason? What approach is better? What do you suggest?
New configurations :

Ayaz_0-1750439370569.png
the previous approach:

Ayaz_1-1750439921953.png

i have attached the project with new configurations 

 
 

标记 (1)
0 项奖励
回复

1,941 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you kept wrong Transfer setting for ch16 and have wrong one for 32byte transfer on ch2. See  attached screenshots for modified setting .

Moreover buffers have to be aligned accordingly as per used transfers

PetrS_0-1750667127203.png

BR, Petr

0 项奖励
回复