S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K344 to enable pinging the lwIP stack from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions. * * Configuration: * - Updated pin configuration * - Modified FXOSC, PLLAUX + dividers * - Platform: added EMAC_0_IRQn interrupt * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Added DIO * * main.c * - Updated only the header * device.c * - No updates * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * ------------------------------------------------------------------------------------------------ * Test HW: MR-CANHUBK344 * MCU: S32K344 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: EMAC <-> RDDRONE-T1ADAPT <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K389 to enable pinging the lwIP stack from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions, except J848, J822, J1136 - disconnected to enable an external debugger. * * TJA1103-SDBR: * mode rev-RMII * CONFIG 0,1 1-2 * CONFIG 2,4 2-3 * CONFIG 3 1-2 * * Configuration: * - Updated pin configuration * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Eth_43_GMAC: configured for RGMII 1G, EthIndex = 0 * - Added DIO * * main.c * - Updated only the header * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * ------------------------------------------------------------------------------------------------ * Test HW: S32K389EVB-Q437 SCH-94080 REV C, 700-94080 REV A * MCU: S32K389 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: GMAC1_SABRE <-> TJA1103-SDBR (rev-RMII mode) <-> RDDRONE-T1ADAPT <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K358 to enable pinging the lwIP stack from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * S32K3X8EVB-Q289: * - All jumpers in default positions except: jumper J685 2-3 * * TJA1120-SDBR: * mode RGMII-ID (both TXC/RXC), Master, Autonomous, XTAL * CONFIG 3 2-3 * CONFIG 5 1-2 * CONFIG 4,6 open * * Configuration: * - Updated pin configuration * - Updated GMAC clocks * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Eth_43_GMAC: configured for RGMII 1G * - Added DIO * * main.c * - Updated only the header * * device.c * - Added RTD workaround for DCMRWF* registers * * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3X8EVB-Q289 SCH-54870 REV C, 700-54870 REV A * MCU: S32K358 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: SABRE <-> TJA1120-SDBR <-> Media converter TE-1402 (1G, Follower) <-> * USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K358 to enable pinging the lwIP stack from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * S32K3X8EVB-Q289: * - All jumpers in default positions except: jumper J685 2-3 * * TJA1103-SDBR: * mode RGMII-ID (both TXC/RXC) * CONFIG 0,1 1-2 * CONFIG 2,4 2-3 * CONFIG 3 open * * Configuration: * - Updated pin configuration * - Updated GMAC clocks * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Eth_43_GMAC: configured for RGMII 100M * - Added DIO * * main.c * - Updated only the header * * device.c * - Added RTD workaround for DCMRWF* registers * * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3X8EVB-Q289 SCH-54870 REV C, 700-54870 REV A * MCU: S32K358 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: SABRE <-> TJA1103-SDBR <-> Media converter TE-1402 (100M, Follower) <-> * USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K388 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions except: jumper J361 must be closed. * - Soldering rework required to connect an external debugger. * See S32K388EVB-Q289_HW_User Manual_A3.pdf, chapter 15 (Errata). * * Configuration: * - Updated pin configuration * - Modified PLLAUX + dividers * - Updated GMACx clocks * - Platform: added GMAC0 interrupts * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Eth_43_GMAC: configured for RGMII 1G, EthIndex = 0 * - Added DIO * * main.c * - Updated only the header * device.c * - Added RTD workaround for DCMRWF* registers * (copied from example S32K388_gptp_ds, S32K3xx gPTP Stack 1.0.0) * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * --------------------------------------------------------------------------------------- * Test HW: S32K388EVB-Q289 SCH-88925 REV A, 700-88925 REV X1 * MCU: S32K388 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: GMAC0 <-> Media converter TE-1402 (1G, Follower) <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
**************************************************************************************************** * Detailed Description:   * * The Flexio I2C driver provides an optional configuration parameter for reducing the number of DMA interrupts * required for transmission that are configured with DMA Optimize option. Instead of being interrupted after each * end of transmitting or receiving a data block or data amount larger than 13 bytes, only one interrupt will be raised to * stop frame and inform to user that the transmission was done. * * More details can be found in "RTD_I2C_UM.pdf", the chapter 3.6.3 FLEXIO DMA Optimize. * ------------------------------------------------------------------------------------------------ * Test HW: S32K3x4EVB-T172 SCH-53148 REV B2 * MCU: S32K344_172HDQFP * IDE: S32DS 3.6.0 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: Lauterbach, P&Emicro * Target: Internal_FLASH * Connections: * FXIO_D10_SCL (J4.19) - LPI2C1_SCL (J3.24) * FXIO_D11_SDA (J4.17) - LPI2C1_SDA (J3.27) ***************************************************************************************************/ Test Result:  
View full article
The script performs secure‑recovery and mass‑erase initialization of locked S32K142 MCUs by keeping the device in system reset (PTA5 RESET_B held low) from the moment of power‑on. Before running the script, connect PTA5 (RESET_B) to VSS, power‑cycle the MCU, and start the script. The script first reads the MDM‑AP Status register to determine the MCU’s security and flash‑ready state, then prompts the user to initiate a mass‑erase operation through the MDM‑AP Control register. After the mass erase completes, the user is instructed to release RESET_B (remove PTA5 from VSS), after which the debugger re‑attaches and displays the flash configuration area at address 0x400. Finally, the script prompts whether the MCU should be reprogrammed from an ELF file, and if confirmed, programs flash, loads the project, and executes it.
View full article
******************************************************************************************** * Test HW: S32K312 EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.6.2 * SDK release: RTD 6.0.0 QLP04 * Debugger: PE Micro * Target: Internal_FLASH ******************************************************************************************** The objective of this demo application is to generate an interrupt and wakeup using the single GPIO. In this application, USR_SW5 (PTB26) in S32K312_Q172 EVB is used both as an interrupt source in RUN mode and as a wake‑up source from STANDBY mode.   Thanks & regards, Krishnakumar V
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + GPT RTC API.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) or S32K344MINI-EVB * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & RTC units for wake-up. The RTC is present in always ON domain, hence available in RUN mode as well as in STANDBY mode.   The chip contains one instance of RTC (Real Time Clock) timer and API (Autonomous Periodic Interrupt) timer, where both can perform 32-bit comparisons. Both RTC and API timers can generate interrupts as well as wake-up from low power modes. The following figure highlights the path for RTC API wake-up. Please refer to Chapter 69.3.2 API functional description from the S32K3XX reference manual (Rev. 12) for further information.   The routine waits for SW5 to be pressed, then: Turns off the green LED Switches CORE_CLK to Option C - Boot Standby mode (CORE_CLK @ 24 MHz). Initializes the ICU driver. Configures RTC_API channel (WKPU0) Initializes GPT module. Starts timer and sets RTC_API_TIME. Enters standby. After the period defined, RTC API generates an interruption and MCU wakes up. After wake-up, MCU resets and polls for SW5 to be pressed again. The RTC API value can be changed with RTC_API_TIME definition. This example is provided as is with no guarantees and no support.
View full article
* Detailed Description: * Updated the example lwip_FreeRTOS_s32K344 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=2ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions * * Configuration: * - Updated pin configuration * - Updated clock configuration * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Added DIO * * main.c * - Updated only the header * device.c * - No changes * test.c * - Commented out the code that shuts down the TCP/IP stack after * its predefined timeout * - Added LED task * * ----------------------------------------------------------------------------- * Test HW: S32K344MINI-EVB SCH-94921 REV B, 700-94921 REV B * MCU: S32K344 * Debugger: On Board * Target: internal_FLASH * EVB connection: EMAC <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
********************************************************************************* * Detailed Description: * Updated the example lwip_FreeRTOS_s32K389 to enable pinging the lwIP stack * from the command window * *ping 192.168.0.209 * *Pinging 192.168.0.209 with 32 bytes of data: *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 *Reply from 192.168.0.209: bytes=32 time=1ms TTL=255 * *Ping statistics for 192.168.0.209: * Packets: Sent = 4, Received = 4, Lost = 0 (0% loss), *Approximate round trip times in milli-seconds: * Minimum = 1ms, Maximum = 2ms, Average = 1ms * * * EVB: * - All jumpers in default positions, except J848, J822, J1136 - disconnected * to enable an external debugger. * * Configuration: * - Updated pin configuration * - Modified PLLAUX + dividers * - Updated GMAC0 clocks * - Platform: added GMAC0 interrupts * - IP address set to 192.168.0.209 and enabled UDP_ECHO, etc. * - Eth_43_GMAC: configured for RGMII 1G, EthIndex = 0 * - Added DIO * * main.c * - Updated only the header * device.c * - Added RTD workaround for DCMRWF* registers * (copied from example S32K389_gptp_ds, SW32K3xx_M7_gPTP_1.1.0_CD01_D2602) * test.c * - Commented out the code that shuts down the TCP/IP stack after its predefined timeout * - Added LED task * * ----------------------------------------------------------------------------- * Test HW: S32K389EVB-Q437 SCH-94080 REV C, 700-94080 REV A * MCU: S32K389 * Debugger: Lauterbach Trace32 * Target: internal_FLASH * EVB connection: GMAC0 <-> Media converter TE-1402 (1G, Follower) <-> * <-> USB-to-Ethernet adapter <-> Laptop DELL, Windows 11
View full article
**************************************************************************************************** * Detailed Description: * * SW triggered conversion of ADC0 internal channel 50 (ANAMUX_OUT). * ANAMUX is used for internal supply monitoring. * Supply to be monitored is configured using DCMRWF1 register. * * PIT is configured to generate interrupt each second then ADC conversion for selected supply is * SW started and measured result is printed to the UART interface * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3x4EVB-T172 Rev B * MCU: S32K344_172HDQFP * IDE: S32DS 3.6.0 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: Lauterbach, P&Emicro * Target: Internal_FLASH * Serial: 115200, 8N1 ***************************************************************************************************/ Terminal output
View full article
S32K1 vdd falling low voltage POR clear situation 1. Abstract This document primarily aims to explain the situation where the POR flag in the RCM_SSRS of the S32K1 chip is cleared, and to explain the setting status of the reset pin and the POR and LVD bits when VDD is powered down. This article is written because some customers, when using the RCM_SSRS reset flag to determine the corresponding RAM initialization conditions, have made incomplete considerations, leading to component failures in actual projects. They mistakenly believe that as long as the SSRS POR flag is not cleared by software writing a 1 after power-on, the POR bit will remain indefinitely. In reality, even after power-on, if subsequent power fluctuations cause VDD to drop to LVD/LVR and trigger a reset, the POR flag may still be automatically cleared by the chip.   2. Document content This article mainly categorizes VDD power-down scenarios into three main types: (1) VDD drops below the minimum LVR value but above VPOR, and then power is  back to normal VDD. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. (2) VDD drops below LVD, above LVR, and LVDRE=0. In this case, reset flag POR=1 and LVD=1 in RCM_SSRS. (3) VDD drops below LVD, above LVR, and LVDRE=1. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. The schematic diagram is as follows:   3. Test result on S32K116 board        
View full article
This is set of S32K389EVB-Q437 demo projects. S32K389_GPIO_RTD6d0_S32DS3d6d2 S32K389_LPUART_RTD6d0_S32DS3d6d2 S32K389_FlexCAN_RTD6d0_S32DS3d6d2 S32K389_PFLASH_RTD6d0_S32DS3d6d2 S32K389_ADC_RTD6d0_S32DS3d6d2 S32K389_eMIOS_GPT_RTD6d0_S32DS3d6d2 S32K389_LowPower_RTD6d0_S32DS3d6d2 Examples are based on S32K3 RTD version 6.0 and created in S32DS version 3.6.2
View full article
NXP has ported FreeRTOS SMP (V11.1.0) to the S32K389. Many customers are interested in how to enable the FreeRTOS SMP on the S32K3xx. The demo is implemented as a single project with a single linker file and a single ELF file. Demo SW/HW Environment: 1. S32DS3.6.4 2. RTD7.0 3.SW32K3_FreeRTOS_11.1.0_7.0.0_CD1_HF1_D2511_DesignStudio_updatesite 4. S32K389 EVB  Demo Code Key Features: 1.FreeRTOS SMP is running on the S32K389 with all cores active. 2.DTCM is used as the task stack. 3.The hardware semaphore (SEMA42) is enabled in FreeRTOS. 4.XRDC is enabled so that each core has a unique core ID for semaphore operations. 5.CAN0 runs on Core0, and CAN4 runs on Core2. 6.LPUART11 is used to print debug information. All cores can output their own messages via LPUART11.  Disclaimer: The code is provided as demo code. NXP makes no commitment regarding its quality.  
View full article
Lauterbach FCCU_Utility plugin - S32K3xx MPC57xx_FCCU_Utility_rev0.pdf This Lauterbach debugger plugin alows user to use FCCU configurations directly from debugger interface. Such will speed up development and will not require to recompile and program project each time FCCU configuration is changed.   The supplied document describes how to use Lauterbach FCCU (fault collection and control unit) periphery extension for S32K3xx devices. It is expected that user has deep knowledge on FCCU mechanisms in order to effectively use this extension. In such case this debugger plugin could be of a great value for various use cases like FA or debugging in development. Best regards, Peter
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + SIUL2.  ------------------------------------------------------------------------------ * Test HW: S32K312EVB-Q172 (SCH-50892 REV B) * MCU: S32K312 * IDE: S32DS v3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up and defines a section in linker file for 32KB of Standby RAM. How to use Standby RAM? Modify the linker file to separatethe 32KBstandby RAM(0x2040 0000 ~0x2040 8000) from int_sram memory region, and place standby .bss and .data or .text sections into the new region as well as adjust the link address symbols for customized initialization during startup. Initialize the standby RAM only if it’s Power-On Reset. Use key word attribute to define the variable/function in relevant memory section. Counter variable is placed in standby ram section: __attribute__ ((section (".sram_standby_bss"))) volatile int RunStandbyCounter0 = 0; Linker file (.ld) must be modified accordingly. Standby sections and link address symbols must be placed: MEMORY { int_pflash : ORIGIN = 0x00400000, LENGTH = 0x001D4000 /* 2048KB - 176KB (sBAF + HSE)*/ int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */ int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00008000 /* 32KB */ int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0000F000 /* 60KB */ int_stack_dtcm : ORIGIN = 0x2000F000, LENGTH = 0x00001000 /* 4KB */ int_standbysram : ORIGIN = 0x20400000, LENGTH = 0X00000100 /* standby ram 256B*/ int_sram : ORIGIN = 0x20400100, LENGTH = 0x00007E00 /* 32KB - 0x100, needs to include int_sram_fls_rsv*/ int_sram_fls_rsv : ORIGIN = 0x20407F00, LENGTH = 0x00000100 int_sram_no_cacheable : ORIGIN = 0x20408000, LENGTH = 0x00007F00 /* 32KB , needs to include int_sram_results */ int_sram_results : ORIGIN = 0x2040FF00, LENGTH = 0x00000100 int_sram_shareable : ORIGIN = 0x20410000, LENGTH = 0x00008000 /* 32KB */ ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */ } ... .sram_standby (NOLOAD): { . += ALIGN(4); *(.sram_standby_bss) } > int_standbysram ... __STANDBY_SRAM_START = ORIGIN(int_standbysram); __STANDBY_SRAM_SIZE = LENGTH(int_standbysram); Note 1: RAM ECC must be initialized only if it’s Power-on Reset. Note 2: CM7 CPU D-Cache MUST be disabled to use the Standby RAM area. Or set the standby RAM(0x2040 0000 ~0x2040 8000) as non-cacheable in MPU configuration. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Disables D-Cache. Initializes RAM ECC (if reset was Power-on Reset). Adds +1 to the standby counter placed in Standby RAM. Switches core clock to FIRC. Initializes the WKPU instance. Configures WKPU42 (PTB19). Enters standby. If SW6 is pressed, MCU will perform a software reset through the Power_Ip_PerformReset() API. After wake-up, MCU resets and polls for SW5 to be pressed again. In this application, LPUART6 (connected to USB OpenSDA interface) is enabled and will show previous reset reason (external reset, power-on reset, wakeup, functional reset), as well as printing standby counter between resets/standby cycles. Connect a USB cable to J40, and open a Serial terminal on PC for the serial device with these settings:   9600 baud rate   No parity   One stop bit  No flow control   After either a SW reset, or a wake-up cycle, the standby counter will increase. If a destructive reset or Power-on Reset is asserted, the counter is reset.    This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of ICU (WKPU) + DIO (GPIO).   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up. This is the simplest WKPU example. Pin PTB19 (WKPU42) is configured for wake-up.  The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Turns off green LED Switch system clock to FIRC (Option C - Boot Standby mode @24MHz). Initialize the Icu driver. Configures WKPU42 (PTB19). Enters standby. After pressing SW6, MCU wakes up, resets and polls for SW5 to be pressed again. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of ICU (WKPU) + CAN.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This project configures both Can_43_FLEXCAN and CanIf modules for CAN communication, along with the ICU (WKPU) module for wake-up. Transmission is done via POLLING, while reception is configured via INTERRUPT.  Tx MB is set to STD ID 123h. Acceptance mask is set to 0x0 (accept all IDs). CAN messages are sent using Can_43_FLEXCAN_Write() and received using the CanIf_RxIndication() callback. After CanIf_bRxFlag is set, an ACK message is sent back. If TJA1153 transceiver is used, macro TJA1153_EVB_TRCV must be used. If not, use TJA1043_EVB_TRCV for standard transceiver initialization (CAN0_STB & CAN0_EN pins set to HIGH).  FlexCAN bitrate is calculated with: CAN bit timing calculator sheet. CAN classic (non-FD) 24Mhz clock 500Kbps 81.3% Sample Point Main routine: Waits for SW5 to be pressed, or for FlexCAN Rx interrupt. If SW5 is pressed, turns off green LED, disables FlexCAN and switches CORE_CLK to FIRC. It then configures PTA6 (CAN0_RX) for wakeup. If a CAN message is received (edge detect on PTA6), MCU wakes up and will enter main routine again. If a CAN frame is received, MCU will wake-up and wait for SW5 to be pressed again. Note: The first CAN frame may not be fully received since there will be some time for the MCU to warm up from STANDBY mode back to RUN mode, so the application may need to ignore the first CAN frame. Note 2: In order to test this example, another CAN node must be connected to CAN0_OUT. This example is provided as is with no guarantees and no support.
View full article
***************************************************************************** *Detailed Description: *This example will show you how to configure Wdg_fs23 Driver. *Sbc_fs23_InitDriver, Sbc_fs23_GoToInitState, Wdg_43_fs23_Init, Sbc_fs23_InitDevice initialize the Sbc device and external Wdg in SLOW MODE(This mode can e.g. be used during system startup/initialization phase). *Sbc_fs23_InitDevice release FS0B, according to the configuration in Sbc_fs23 WatchdogConfig tab: Release safety outputs after init *Sbc_fs23_TimeDelay delay for an amount of time, allow Gpt ISR to trigger watchdog externally. *Wdg_43_fs23_SetMode(WDGIF_FAST_MODE); switch Wdg operation mode to FAST MODE(This mode can e.g. be used during normal operations of the ECU). *Wdg_43_fs23_SetTriggerCondition(10000U); sets a new timeout value to 10 seconds, during which Wdg_fs23_Cbk_GptNotification0 continuously refresh the watchdog. *To demonstrate the watchdog timeout, Wdg_43_fs23_SetTriggerCondition was not called again to set a new timeout value, and Wdg_fs23_Cbk_GptNotification0 no longer refreshed the watchdog. *The watchdog error counter(WD_ERR_CNT) continues to increase reached its maximum value(WD_ERR_LIMIT), causing fault error counter(FLT_ERR_CNT) to increment by 1. *FS23 eventually enters fail-safe mode because FLT_ERR_CNT >= max. At this point, it was observed that LEDs V1 (D7), V2 (D8), and V3 (D9) of KITFS23SKTEVM were turned off. *The SPI data between FS23 and S32K311 are captured and attached to the project. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * RTD_WDG_43_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Wdg_43_fs23_TS_T40D34M10I0R0\doc * AUTOSAR_SWS_WatchdogDriver.pdf https://www.autosar.org/fileadmin/standards/R21-11/CP/AUTOSAR_SWS_WatchdogDriver.pdf * This example is migrated from Wdg_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 *****************************************************************************
View full article