S32K311 UART Idle state Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K311 UART Idle state Interrupt

S32K311 UART Idle state Interrupt

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 UART IP Driver for the S32K3xx MCU.

 The example uses LPUART0 for transmit 20 packets with each packet of 21 bytes using the Interrupt in cyclic order. Also when receiving UART packet generate Idle interrupt when variable length of data is received.

I used coolterm tool to send the string of data. If Data send by cool term is less than 20 bytes which is set by API call Lpuart_Uart_Ip_AsyncReceive(), then Ideal interrupt is received

RTD driver modified in RTD --> Lpuart_Uart_Ip.c.

Baudrate : 921600
 ------------------------------------------------------------------------------
* Test HW: S32K31XEVB-Q100
* MCU: S32K311
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1713853153843.png


Idle Interrupt received :--

Dinesh_Guleria_1-1713853788454.png

 

 

附件
无评分
版本历史
最后更新:
‎04-22-2024 11:56 PM
更新人: