*******************************************************************************
The purpose of this demo application is to present a usage of the
UART IP Driver for the S32K3xx MCU.
The example uses LPUART6 for transmit & receive five bytes using the DMA.
------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-T172
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************
Dinesh_Guleria_0-1718197381145.png
Dinesh_Guleria_1-1718197381161.png
Putty output :--
Dinesh_Guleria_2-1718197434242.png