Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500

Example S32K344 SPI Transmit & Receive Using DMA DS3.5 RTD500

*******************************************************************************************************

* Detailed Description:

The purpose of these demo applications is to present a usage of the LPSPI Driver together with DMA Driver (IP and MCAL) for the S32K3xx MCU.

The applications uses the LPSPI driver to transfer data between LPSPI2 (master, no DMA) and LPSPI0 (slave, with DMA) physical units.

* Connections

VaneB_0-1731361492724.png


* Test HW: S32K3X4EVB-T172
* MCU: S32K344
* Debugger: S32DS 3.5, PEMicro Multilink Universal FX rev.B
* Target: internal_FLASH
*******************************************************************************************************

Attachments
No ratings
Version history
Last update:
‎11-11-2024 02:48 PM
Updated by: