Example S32K324 I2C Transmit & Receive Using DMA DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K324 I2C Transmit & Receive Using DMA DS3.5 RTD300

Example S32K324 I2C Transmit & Receive Using DMA DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
LPI2C-0 as MASTER and LPI2C-1 Slave, using DMA for TX & RX for the S32K324 MCU.


 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q257
* MCU: S32K324
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1709199728594.png

 

Dinesh_Guleria_1-1709199772913.png
附件
无评分
版本历史
最后更新:
‎02-29-2024 02:47 AM
更新人: