Example S32K312 SWT DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K312 SWT DS3.5 RTD300

Example S32K312 SWT DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 SWT IP Driver for the S32K3xx MCU.

 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

With S32K312 device take care, HSE clock AIPS_SLOW_CLOCK ratio,  kept 1:2 :--

Dinesh_Guleria_0-1706855323004.png

 


The example we use to trigger the SWT once & go to while(1) loop.
This will trigger the watchdog RESET.

Dinesh_Guleria_1-1706855535347.png



Then After RESET from SWT we will check at starting of main function, if RESET reason is SWT, then glow LED and wait in while(1) loop  :--

Dinesh_Guleria_2-1706855589096.png

 



附件
无评分
版本历史
最后更新:
‎02-01-2024 11:35 PM
更新人: