Example S32K312 ADC_IP Continuous Scan DMA S32DS36 RTD600

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K312 ADC_IP Continuous Scan DMA S32DS36 RTD600

Example S32K312 ADC_IP Continuous Scan DMA S32DS36 RTD600

* ==================================================================================================
* Detailed Description:
*
* This example shows how to implement ADC continuous scan with DMA read.
* ADC1 is set to perform continuous scan of 4 channels (S10/S11/S12,S13) with DMA request enabled
* for last channel S13. DMA reads respective sequential ADC data registers in one major loop.
*
* ADC1 channel S10 is connected to board's potentiometer, converted value is used to dim board's LED.
*
* ==================================================================================================
* Test HW: S32K312EVB-Q172
* MCU: S32K312_172LQFP
* Compiler: S32DS 3.6.3
* RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
* Debugger: On-Board Debugger (J40), Lauterbach
* Target: Internal_FLASH
* ==================================================================================================

 

Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty
express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to
the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications
or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP
regarding the Materials may be used by NXP without restriction.

 

Attachments
No ratings
Version history
Last update:
‎09-29-2025 11:50 PM
Updated by: