Example S32K116 WDOG Fast Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K116 WDOG Fast Test

Example S32K116 WDOG Fast Test

************************************************************************************************
Detailed Description:
WDOG tested in SystemInit() function (system_S32K116.c) after POR.
For debugging purposes:
- WDOG counter reference clock is pre-scaled to slow the test (CS_PRES = 1).
- During CNT_LOW test, BLUE LED (PTE8) ON.
- During CNT_HIGH test, RED LED (PTD16) ON.
- Once both tests have passed, GREEN LED (PTD15) ON.
If either of the test fails, WDOG will stay in its default configuration and rest the MCU.
----------------------------------------------------------------------------------------------------------------
Test HW: S32K116EVB-Q048 REV.B
MCU: S32K116 0N96V
Debugger: S32DSR1, OpenSDA
Target: internal_FLASH
************************************************************************************************

Attachments
Comments

Hi Daniel, 

Just a question from my side: out of reset the WDOG is unlocked, so why are you unlocking the wdog in reconf?

What does happend if wdog is already unlocked and we are unlocking it?

thanks and best regards, 

L.

Hi,

The unlock write is indeed unnecessary since CS_ULK = 1 our of reset.

Nothing happens, it unlocks already unlocked WDOG registers and continues.

Regards,

Daniel

Hi Daniel,

Can I apply this example for S32K144EVB?

Hi [email protected],

Yes, it has the same WDOG module.

BR, Daniel

100% helpful (1/1)
Version history
Last update:
‎11-27-2018 05:07 AM
Updated by: