*******************************************************************************
The purpose of this demo application is to present a usage of the
EMIOS IP Driver in Polling mode for the S32K3xx MCU.
The example use to :--
EMIOS-1 - ch-0 --> PTC24 --> Generate the PWM
EMIOS-1 - ch-1 --> PTC25 --> is the ICU channel to measure the duty
Pins used :--
Dinesh_Guleria_0-1733896956186.png
Dinesh_Guleria_4-1733897197653.png
Dinesh_Guleria_5-1733897299281.jpeg
This example is tested for IPWM mode . :--
Dinesh_Guleria_0-1733898410969.png
IPWM mode , ICU Driver User Manual :--
Dinesh_Guleria_2-1733897086528.png
Result :--
Dinesh_Guleria_1-1733898628922.png
------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************