when I disable EcucPostBuildVariants in EB tresos, many errors occur

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

when I disable EcucPostBuildVariants in EB tresos, many errors occur

2,153 次查看
lihua
Contributor I

when i disable the EcucPostBuildVariants under module EcuC in EB tresos 27, many errors occur. the error is “The variant attribute of the node /AUTOSAR/TOP-LEVEL-PACKAGES/Can_43_LLCE/ELEMENTS/Can/CanConfigSet/CanHardwareObject/CanHardwareObject_9/CanIdType refers to selectable criterions, but no selectable is currently active.“ what should i do to solve these problems?

the mcal I used was S32G2XX_LLCE_GATEWAY_1.0.1_HF1_D2106

 

errorcode95034.jpgerrorcode95034_2.jpg

0 项奖励
回复
3 回复数

2,102 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello lihua,

You may want to install the S32G_LLCE_GATEWAY_1.0.2_HF2_D2109 since the version you are using has a lot of malfunctions like this.You can download it from:

https://www.nxp.com/app-autopackagemgr/software-package-manager:AUTO-SW-PACKAGE-MANAGER#

 

Regards

0 项奖励
回复

2,078 次查看
lihua
Contributor I

I have tried S32G_LLCE_GATEWAY_1.0.4_D2204, the same errors occured

90 次查看
wei_zhoucq
Contributor II
我也遇到了这个类似的问题,将其余项目的XDM文件复制到另外一个项目就会出错,请问你解决了吗?
0 项奖励
回复