uboot ncore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot ncore

1,756件の閲覧回数
shiyiheng
Contributor III

I have a network transmission problem under uboot. Does ncore work under uboot?

0 件の賞賛
返信
3 返答(返信)

1,722件の閲覧回数
shiyiheng
Contributor III

I had some problems debugging multicore, then I verified cache consistency between two clusters under uboot, and I found that every time the two clusters communicated with each other, 0x140 bytes did not align, and other data was normal.

shiyiheng_0-1718965749780.png

 

0 件の賞賛
返信

1,703件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Based on S32G3 reference manual chapter 75 Error Injection Module (EIM), not to support Ncore internal RAM error injection.

Checked the sCheck test target, it support NCORE_RCCU, not support Ncore internal RAM Ecc test.

Regards

0 件の賞賛
返信

1,666件の閲覧回数
shiyiheng
Contributor III

I try to test with the core0 of cluster0 and core0 of cluster1. The test steps are as follows:
1 core0 of cluster0 writes 0x66666666 to 0x80000000 to 0x80000400
The core0 of 2 cluster1 reads 0x80000000 to 0x80000400
3 core0 of cluster1 writes 0x99999999 to 0x80000200 to 0x80000400
4 core0 of cluster0 writes 0x99999999 to 0x80000000 to 0x80000400
In theory, the core0 of cluster1 should be able to read 0x666666666 in the address range of 0x80000000~0x80000400, but the world did not read it, I guess it may be because the address state machine is M, ncore did not move. At the same time, the core0 of cluster0 does not read 0x99999999, for a similar reason.

shiyiheng_0-1719224484261.png

shiyiheng_1-1719224552569.png

 


Question:
How do I verify that ncore takes effect in uboot

 

0 件の賞賛
返信