Using a watchdog in the uboot does not take effect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using a watchdog in the uboot does not take effect

1,449件の閲覧回数
shiyiheng
Contributor III

I want to use a watchdog under uboot, but the watchdog doesn't work, the command is as followsshiyiheng_0-1718854066596.png

Do you need any other configuration?

0 件の賞賛
返信
3 返答(返信)

1,421件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @shiyiheng, 

Thank you for contacting NXP Support!

Could you please help me with your information about processor and BSP version?
Additionally, are you trying any guides or manuals as reference to use the watchdog?

0 件の賞賛
返信

1,412件の閲覧回数
shiyiheng
Contributor III

I am using the S32G platform, I have used several BSP versions to try such as BSP34, in the kernel according to the above operation watchdog is normal, in the uboot watchdog did not reset the system?

0 件の賞賛
返信

1,386件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @shiyiheng, 

Have you tried any modifications on Uboot build process?
It seems that the watchdog requires a specific configuration on Uboot to enable and set the time. This configuration should be enabled by default on that BSP version; however, I'm still working with the team to confirm that.

0 件の賞賛
返信