sCheck shutdown tests failing on Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sCheck shutdown tests failing on Application

577 Views
msoddu2
Contributor I

Hi,
the execution of some sCheck shutdown test on Application is failing (the test signature is showing a value great then 0 in the LSB 16 bits).

Is it possible to understand the reason why it is failing?

Here are the screenshots of the faulty tests.

1)

sCheck.Sram_EccStartupTest.SRAM_0_ECC.Signature.0xB6A90000.png

2) 

sCheck.CmuFm_Test.CMU_FM_4.Signature.0xDAD00000.png

3) 

sCheck.CmuFm_Test.CMU_FM_3.Signature.0xDACD0000.png

Thanks in advance!

#SV62 #S32G3

0 Kudos
Reply
4 Replies

437 Views
msoddu2
Contributor I
 
0 Kudos
Reply

528 Views
msoddu2
Contributor I

Hello Joey,
the sCheck_ExecuteShutdownTests function just returns a value related to the function execution itself, that's why I was focused to debug the "inside" functions.
In fact I posted some screenshots showing that the test Signature contained the 16 LSB of it with a value not egual to 0.

to be more clear, why I get the following signatures:

  1. 0xB6A90004 (what is it the meaning of the last 4)
  2. 0xDAD00001 (what is it the meaning of the last 1)
  3. 0xDACD0001 (what is it the meaning of the last 1)


Thanks!

0 Kudos
Reply

493 Views
Joey_z
NXP Employee
NXP Employee

hi,msoddu2

Thank you for your reply.

Refer to the sCheck user manual and the perspective of the program, these values of yours are Accumulate signatures. If all tests are executed successfully, it should be equal to ExpectedSignature.

Joey_z_0-1750662031122.png

Hope it can help you.

BR

Joey

 

0 Kudos
Reply

542 Views
Joey_z
NXP Employee
NXP Employee

hi,msoddu2

Thank you for contacting us.

You can try to check the Shutdown test in the sCheck_ExecuteShutdownTests function. The function includes sCheck_ExecuteSimpleTestBatch.

Joey_z_0-1750401837222.png

Hope it can help you.

BR

Joey

0 Kudos
Reply