S32G Bootable SD Card Setup – BSP Version Clarification Needed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G Bootable SD Card Setup – BSP Version Clarification Needed

867件の閲覧回数
yonghwa_seo
Contributor I

I'm trying to find the correct Linux BSP for the S32G platform.
I want to create a bootable SD card for the S32G-VNP-RDB2 board.
However, on the software download page, only Linux BSP 23.5 is available.
From what I understand, Linux BSP 23.5 seems to be intended for S32V series, not for S32G.
Where can I download the appropriate Linux BSP for the S32G platform?
Also, is it possible to use Linux BSP 23.5 to boot an S32G board?
Thank you in advance.

 

0 件の賞賛
返信
1 返信

834件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @yonghwa_seo 

Thanks for your post.

No, it is not for the S32G product.

For downloading the BSP images, it is suggested accessing the following URL:

https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER

chenyin_h_0-1750862973255.png

Some other BSP version listed could also be downloaded via this page, I hope it will help.

 

BR

Chenyin 

 

0 件の賞賛
返信