pwm dts setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pwm dts setup

1,204件の閲覧回数
shiyiheng
Contributor III

s32g BSP34

I want to use the pwm of a53, I found that the device tree is as follows configuration 1+2, I try to configure only 1 to achieve PWM. However, the use cases of the device tree are all 1+2, what is the function of the following screenshot 2 configuration?

shiyiheng_0-1721698515387.png

 

0 件の賞賛
返信
1 返信

1,172件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the following question:

what is the function of the following screenshot 2 configuration?

Is it used to configure the FlexTimer channel as an input. For more information on regards of the different features available under the FlexTimer on regards of inputs, we can recommend looking into the respective S32G Reference Manual into the FlexTimer Chapter.

Please, let us know.

0 件の賞賛
返信