How to encypt with AES algo on #S32G3 - RDB3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to encypt with AES algo on #S32G3 - RDB3

309 Views
Liuliyuan
Contributor I

Hello,

We are trying to test AES encrypt and decrypt function with the HW of HSE on RDB3 board. We tried PKCS11-tool and Opnessl , none  worked. Could you please help have a check?

  1. PKCS11-tool

 ~/pkcs11-tool\                                                                                           

>  --module /usr/lib/libpkcs-hse.so.1\                                                                                             

>  --encrypt\                                                                                                                      

>  --mechanism AES-CBC\                                                                                                            

>  --id 000101 \                                                                                                                   

>  --iv 0123456789abcdef0123456789abcdef\                                                                                          

>  --input-file file1.txt\                                                                                                         

>  --output-file file1_pkcs11.dat                                                                                                  

libhse: initialized, firmware status 0x6b20                                                                                        

Using slot 0 with a present token (0x0)                                                                                            

Using encrypt algorithm AES-CBC                                                                                                    

libhse: service response 0xA5AA5317 on channel 5                                                                                   

libhse: read reply failed on channel 5                                                                                             

libhse: closed                                                                                                                     

error: PKCS11 function C_EncryptUpdate failed: rv = CKR_FUNCTION_FAILED (0x6)                                                      

Aborting.                                                                   

2. OPENSSL

2.1 With -K parameter, key is provided directly.  One failure reported and one blank file created. The log as below:

 openssl enc -engine pkcs11 -aes-128-cbc -in file1.txt -out file1_HWenc.dat -iv 0123456789ABCDEF0123456789ABCDEF  -K 0123456789ABCDEF0123456789ABCDEF -debug                                                                                  

Engine "pkcs11" set.                                                                                                               

ctx_load_object returned NULL                                                                                                      

BIO[0x55ad1bd370]: ctrl(6) - cipher                                                                                                

BIO[0x55ad1bd2a0]: ctrl(6) - FILE pointer                                                                                          

BIO[0x55ad1bd2a0]: ctrl return 0                                                                                                   

BIO[0x55ad1bd370]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: ctrl(10) - FILE pointer                                                                                         

BIO[0x55ad1bd030]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: ctrl(2) - FILE pointer                                                                                          

BIO[0x55ad1bd030]: ctrl return 0                                                                                                   

BIO[0x55ad1bd030]: read(0,8192) - FILE pointer                                                                                     

BIO[0x55ad1bd030]: read return 1 processed: 367                                                                                    

BIO[0x55ad1bd370]: write(0,367) - cipher                                                                                           

BIO[0x55ad1bd370]: write return 0 processed: 0                                                                                     

error writing output file                                                                                                          

BIO[0x55ad1bd030]: Free - FILE pointer                                                                                             

BIO[0x55ad1bd2a0]: Free - FILE pointer                                                                                             

BIO[0x55ad1bd370]: Free - cipher           

 

2.2 When we try to load key from HW, we cannot find a right parameter to use. -inkey/-key/-keyform are not supported on "openssl enc"

 

Many thanks.

0 Kudos
Reply
3 Replies

289 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We assume that you are trying to implement this under Linux, is this correct?

If so, can you let us know which BSP version are you using?

Please, let us know.

 

0 Kudos
Reply

280 Views
Liuliyuan
Contributor I
Hi,
Yes,we are working on Linux. The BSP version is 40.0.
Thanks
0 Kudos
Reply

259 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. 

All information on regards of HSE/Crypto usage under BSP40 are provided under the BSP40 User Manual for S32G3 platform.

Aside from that, we are not seeing much information on regards of PCKS11 and openssl usage, since we understand is not supported directly by NXP. For that, we can recommend contacting the related support team.

We do apologize.

Please, let us know.

0 Kudos
Reply