llce_sample_app_pfe ETH2CAN problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

llce_sample_app_pfe ETH2CAN problem

ソリューションへジャンプ
6,055件の閲覧回数
seeu
Contributor III

Hi,

I use llce_sample_app_pfe to run ETH2CAN can't work normally, Because I can't receive the  CAN frame normally. But in this sample I can get the acf-can frame,whether this routine can only implement CAN2ETH, but not ETH2CAN?

Also, in data.dump debug_buff, there are some information  Client's (1) RX queue is full. Frame dropped. Is this normal phenomenon?

Snipaste_2023-07-13_09-59-15.pngSnipaste_2023-07-13_09-59-15.png

Snipaste_2023-07-13_09-59-51.pngSnipaste_2023-07-13_09-59-51.png

  

0 件の賞賛
返信
1 解決策
5,402件の閲覧回数
seeu
Contributor III

Hi,

I chang the value from 72 to 73, and re-open trace32 GUI, now it can run normally.But I don't know why I fail last time.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
6,043件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which RTD/LLCE/PFE version are you using? Also, are you using any NXP platforms? Or is this a custom board?

Please, let us know.

0 件の賞賛
返信
6,027件の閲覧回数
seeu
Contributor III

hi,

SW32G_RTD_4.4_3.0.2, S32G_LLCE_1_0_4, PFE-DRV_S32G_M7_MCAL_BETA_0.9.7, target board S32G-VNP-RDB2.

0 件の賞賛
返信
6,011件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information. Ther are 2 known-issues under the above mentioned LLCE v1.0.4 example. One is the ETH2CAN buffer configurations.

Have you done any modifications to the project?

The ETH2CAN buffer config change is the following:

DanielAguirre_0-1689365832002.pngDanielAguirre_0-1689365832002.png

 

Please, let us know.

0 件の賞賛
返信
5,505件の閲覧回数
seeu
Contributor III

Hi, 

I chang the value from 72 to 73, now the frame drop problem were solved. But I can't still receive the can frame from ETH2CAN. Because I comment the CAN2ETH code, and use tcpreplay to send the ETH packet to PFE_MAC1(P3A connector),and run the code,  Logic analyzer can't receive CAN frame, and the variable rxIndicationCount=0 .

Snipaste_2023-07-17_16-58-22.pngSnipaste_2023-07-17_16-58-22.png

Snipaste_2023-07-17_16-35-35.pngSnipaste_2023-07-17_16-35-35.png

  

0 件の賞賛
返信
5,459件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

The recommended way of doing the ETH2CAN channel is to select the UDP packet being sent with the CAN2ETH feature then sending it back:

DanielAguirre_0-1690225805329.pngDanielAguirre_0-1690225805329.png

Is this what you are doing?

Please, let us know.

0 件の賞賛
返信
5,438件の閲覧回数
seeu
Contributor III

Hi,

Thanks, I have solved this problem.

5,427件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Was it related to the previous comment?

Still, good to know you got it working.

Please, let us know.

0 件の賞賛
返信
5,403件の閲覧回数
seeu
Contributor III

Hi,

I chang the value from 72 to 73, and re-open trace32 GUI, now it can run normally.But I don't know why I fail last time.

0 件の賞賛
返信
5,384件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the confirmation. It indeed sounds odd, but good to know you got it working.

Have a great day.

0 件の賞賛
返信