goldvip sample project file.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

goldvip sample project file.

Jump to solution
3,093 Views
youngdae
Contributor III

Hello

I use S32G-VNP-RDB2.

I am testing using GoldVIP-1.1.0.

If you look inside the C:\NXP\S32G2-GoldVIP-1.1\GoldVIP-1.1.0-binaries\binaries folder,

There are boot-loader and goldvip-gateway.bin file, but the sample project cannot be found.

Can you provide sample project files and source code to me?

youngdae_0-1652871812840.png

 

 

Labels (1)
0 Kudos
Reply
1 Solution
3,058 Views
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

View solution in original post

0 Kudos
Reply
4 Replies
3,085 Views
asap
NXP Employee
NXP Employee

hi youngdae,

you may refer to the GoldVIP developer's guide,  chapter 2.1 boot and chapter 2.6.2 CAN gateway provided all the basics. for the code, you could try .../NXP/GoldVIP1.x.x/configuration/ (here below showing what I have got with GoldVIP1.1.0 installed)

asap_1-1652876823942.png

last but not least, in the S32G GoldVIP trainign academy, you found CAN gateway session. in the S32G training academy, you could find S32G2 boot training slides and also LLCE CAN support training. fyi.

 

Albert
0 Kudos
Reply
3,071 Views
youngdae
Contributor III

Thank you for reply.

 

but don't open Project using S32DS.

This is EB Tresos Project.

How to change S32DS Project.

0 Kudos
Reply
3,059 Views
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

0 Kudos
Reply
3,051 Views
youngdae
Contributor III

Thanks for your kind reply.

0 Kudos
Reply