goldvip sample project file.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

goldvip sample project file.

跳至解决方案
3,172 次查看
youngdae
Contributor III

Hello

I use S32G-VNP-RDB2.

I am testing using GoldVIP-1.1.0.

If you look inside the C:\NXP\S32G2-GoldVIP-1.1\GoldVIP-1.1.0-binaries\binaries folder,

There are boot-loader and goldvip-gateway.bin file, but the sample project cannot be found.

Can you provide sample project files and source code to me?

youngdae_0-1652871812840.png

 

 

标签 (1)
0 项奖励
回复
1 解答
3,137 次查看
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,164 次查看
asap
NXP Employee
NXP Employee

hi youngdae,

you may refer to the GoldVIP developer's guide,  chapter 2.1 boot and chapter 2.6.2 CAN gateway provided all the basics. for the code, you could try .../NXP/GoldVIP1.x.x/configuration/ (here below showing what I have got with GoldVIP1.1.0 installed)

asap_1-1652876823942.png

last but not least, in the S32G GoldVIP trainign academy, you found CAN gateway session. in the S32G training academy, you could find S32G2 boot training slides and also LLCE CAN support training. fyi.

 

Albert
0 项奖励
回复
3,150 次查看
youngdae
Contributor III

Thank you for reply.

 

but don't open Project using S32DS.

This is EB Tresos Project.

How to change S32DS Project.

0 项奖励
回复
3,138 次查看
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

0 项奖励
回复
3,130 次查看
youngdae
Contributor III

Thanks for your kind reply.

0 项奖励
回复