goldvip example error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

goldvip example error

Jump to solution
4,229 Views
youngdae
Contributor III

youngdae_0-1652777870665.png

Put the fsl-image-goldvip-s32g274ardb2.sdcard file of goldVIP-1.1.0-binaries into the SD card and stop while uboot is running and run write_goldvip_images was performed.

After all the binaries are written, power off the board, configure the DIP switches for NOR
Flash Boot mode (set SW4.7 to OFF) and then power on the board.

But an error occurred as shown in the figure above.

ERROR: Error: s32_io_setup failed

PANIC at PC : 0x0000000034306858

I don't know why.

Tags (1)
0 Kudos
Reply
1 Solution
4,191 Views
nxf45013
NXP Employee
NXP Employee

Hi,

The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.

Vlad 

View solution in original post

0 Kudos
Reply
4 Replies
4,215 Views
nxf45013
NXP Employee
NXP Employee

Hi, 

This error is usually encountered when the ATF can't read from the SD card. (you can try to remove it and reboot from flash, the same error will occur).

Could you try a different SD card? There seems to be some kind of an issue with the one you are using. 

Vlad

0 Kudos
Reply
4,204 Views
youngdae
Contributor III

Hi.

Thank you for reply.

It works fine when booting from the sd card.
After writing to flash with the sd card, remove the sd card and boot from flash, an error occurs.

0 Kudos
Reply
4,192 Views
nxf45013
NXP Employee
NXP Employee

Hi,

The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.

Vlad 

0 Kudos
Reply
4,175 Views
youngdae
Contributor III

Thank you.

0 Kudos
Reply