goldvip example error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

goldvip example error

ソリューションへジャンプ
4,294件の閲覧回数
youngdae
Contributor III

youngdae_0-1652777870665.png

Put the fsl-image-goldvip-s32g274ardb2.sdcard file of goldVIP-1.1.0-binaries into the SD card and stop while uboot is running and run write_goldvip_images was performed.

After all the binaries are written, power off the board, configure the DIP switches for NOR
Flash Boot mode (set SW4.7 to OFF) and then power on the board.

But an error occurred as shown in the figure above.

ERROR: Error: s32_io_setup failed

PANIC at PC : 0x0000000034306858

I don't know why.

タグ(1)
0 件の賞賛
返信
1 解決策
4,256件の閲覧回数
nxf45013
NXP Employee
NXP Employee

Hi,

The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.

Vlad 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,280件の閲覧回数
nxf45013
NXP Employee
NXP Employee

Hi, 

This error is usually encountered when the ATF can't read from the SD card. (you can try to remove it and reboot from flash, the same error will occur).

Could you try a different SD card? There seems to be some kind of an issue with the one you are using. 

Vlad

0 件の賞賛
返信
4,269件の閲覧回数
youngdae
Contributor III

Hi.

Thank you for reply.

It works fine when booting from the sd card.
After writing to flash with the sd card, remove the sd card and boot from flash, an error occurs.

0 件の賞賛
返信
4,257件の閲覧回数
nxf45013
NXP Employee
NXP Employee

Hi,

The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.

Vlad 

0 件の賞賛
返信
4,240件の閲覧回数
youngdae
Contributor III

Thank you.

0 件の賞賛
返信