enabling external EEPROM driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enabling external EEPROM driver

2,597件の閲覧回数
sandeep3
Contributor I

Hello ,

i am using Gold Vip 1.11.0 package , for my custom build S32g399A board . where i am using ST M95M01-DWMN3

So i have integrated the EEPROM driver in the package but i am not able to enable the external driver reference container which is highlighted below, kindly let me know how to enable this container ,or any dependency related to this .
MicrosoftTeams-image.png

Thanks and Regards

Sandeep

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,584件の閲覧回数
sandeep3
Contributor I

Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?

0 件の賞賛
返信

2,552件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

To access external EEPROM through SPI, we can recommend using the SPI driver available under the RTD, since it provides the basic SPI communication with S32G.

Please, let us know.

0 件の賞賛
返信

2,585件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding the overall inquiry. If so, we do apologize.

The Eep driver itself is used mainly for the uSDHC/eMMC communication under S32G, as told under the Eep Driver User Manual:

DanielAguirre_0-1720449747362.png

For which, we understand that it might not be enabled to interface with an external EEPROM under S32G, but for an SD or eMMC. More information can be found under the User Manual and Integration Manual available under the Eep plugin itself.

Please, let us know.

0 件の賞賛
返信

2,577件の閲覧回数
sandeep3
Contributor I
Hi,

If Eep is not supported, then which driver should i use to access external EEPROM through SPI?
0 件の賞賛
返信