debug error error code is 1303

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

debug error error code is 1303

4,036 Views
JunSeoHan
Contributor I

The following error appears every time I proceed with debugging.

what should I do?

 

The error message says "GTA: Target Access Error." I cannot figure out what the problem is.

I am using an MCU called s32g274a and the S32 Debug Probe, a debugger provided by NXP.

debug_error.PNGdebug_error.PNG

0 Kudos
Reply
4 Replies

3,980 Views
Joey_z
NXP Employee
NXP Employee

Hi,JunSeoHan

Could you share your Debugger configuration information as the following picture?

BR

Joey

0 Kudos
Reply

3,976 Views
JunSeoHan
Contributor I

debug_configuration1.PNGdebug_configuration1.PNG

debug_configuration2.PNGdebug_configuration2.PNG

 The debugger configuration information is as shown in the attached picture.

0 Kudos
Reply

3,963 Views
Joey_z
NXP Employee
NXP Employee

Hi,

Thank you for your reply.

1.Could you test the connection state between S32G with the S32DS debugger as the following picture?

2.Do you use the customer board or the development board?

3.what is your boot configuration when you debug process?

BR

Joey

 

0 Kudos
Reply

3,992 Views
Joey_z
NXP Employee
NXP Employee

Hi,JunSeoHan

Thank you for contacting us.

I will help you to check it.

BR

Joey

0 Kudos
Reply