continous reset on RSTB assertion on NXP(S32G399) Pmic-VR5510

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

continous reset on RSTB assertion on NXP(S32G399) Pmic-VR5510

5,050件の閲覧回数
jvs0473
Contributor I

After PMIC Initialization (VR5510) 

We have observed the fluctuation of RST_B pin in the following scenarios:

i)RSTB_REQ from the PMIC through I2C

ii)on the watchdog maximum error count , configured reaction is fs0b only

ii)OFF MODE REQ from the PMIC through I2C

Can you please help here.

0 件の賞賛
返信
8 返答(返信)

5,029件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

 

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Do you mean that the RSTB pin is not behaving as expected? Could you please share more details?

  1. For example, when the watchdog error counter reaches its maximum value, the Fail-safe reaction on RSTB and/or FS0B is configurable with the WD_FS_IMPACT[1:0] bit field (FS_I_WD_CFG register) during the INIT_FS phase.

How is the WD_FS_IMPACT bit configured?

  1. How is your watchdog configured?
  2. Could you please share your RSTB pin configuration (schematic)?

Regards,

David

0 件の賞賛
返信

5,011件の閲覧回数
jvs0473
Contributor I

Hello,

The above following scenarios has been tested individually.

WD_FS_IMPACT - FS0B only is asserted if WD error counter = WD_ERR_LIMIT[1:0]
 WD_FS_IMPACT - FS0B and RSTB are asserted if WD error counter = WD_ERR_LIMIT[1:0]
In both these cases we observed the same behavior. Reset pin is going to low(0v) and high(3.3v)

2)Watchdog is configured with 12ms window period with DC(68.75%, 31.25%) , Error limit - 8
3)

PMIC 

kavya23_3-1697605239674.png

S32G

kavya23_4-1697605268853.png

B is connected to LDO3_S32G in the below screenshot. 

kavya23_5-1697605332055.png

Please help to analyze why RSTB pin is fluctuating instead of going to Reset

 

 

 

 

0 件の賞賛
返信

4,994件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello kavya23,

Once again, thank you for using the NXP community.

As we know, the RSTB is an open-drain output that can be connected in the application to the MCU's RESET pin. RSTB requires an external pull-up resistor to VDDIO or VPRE and a filtering capacitor to GND for immunity.

Finally, could you please share the pull-up resistor value on the RSTB pin?

Regards,

David

0 件の賞賛
返信

4,973件の閲覧回数
jvs0473
Contributor I

Hello,

Thank You for Replying.

External register of 2K Ohm to VPRE has been provided.

kavya23_0-1697690977743.png

The time between the RSTB pin low and high is 4s approx. which is same as Auto Re-try Timeout set via OTP and hence providing expected behavior.
The issue we are not understanding is why it is going to Deep Fail State after the first Reset. Somehow the RSTB is not released after the Reset REQ from PMIC or from S32G or due to WD error count =WD Error Limit.

0 件の賞賛
返信

4,873件の閲覧回数
jvs0473
Contributor I

Hello,

Sorry for the late response.

1. It is reproducible on other boards also.

2.Waveform(screenshot) is attached below. RSTB_DUR bit is configured to 0(10ms)

3. Even though FLT_ERR_IMPACT is configured to No effect on RSTB and FS0B, observed the same behavior on RSTB REQ or OFF Mode Request

image.pngjvs0473_1-1698335458038.png

 

0 件の賞賛
返信

4,856件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello jvs0473,

Please review the response from our specialist below:

This is expected behavior.

RSTB and FS0B are both asserted when no watchdog refresh in INIT_FS.

The device will go into Deep-FS mode when fault error count reach to limit=6 default.

Please check the page50 to Page 55 in attached slides, especially page53 for Watchdog operation mechanism.

diazmarin09_0-1698429388638.png

 

The WD_INIT_TIMEOUT_OTP in customer OTP was set to 1024ms according to their test waveforms.

diazmarin09_1-1698429417336.png

 

Customer needs to refresh the WD before INIT_FS timeout. They can enter debug mode during the develop stage. Please check page26 to page30 for more details of debug mode and Deep-FS mode.

Please review the document that I shared with you (it is confidential). 

Please let me know if there is anything unclear. Thanks.

I hope this information will be useful for you. 

Regards,

David 

0 件の賞賛
返信

4,948件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Your patience is greatly appreciated.

Please review the response from our specialist below:

 

1. This behavior can be captured on only one board, or can be reproduced on different board? Can customer try on another board?

 

2. Can customer show us the waveform of the fluctuation of RST_B pin (instead of reset).   Do they mean they only can see a RSTB low pulse but not RSTB maintaining low?

RSTB is asserted low for about 1ms or 10ms(configurable with RSTB_DUR bit) after RSTB_REQ request or OFF MODE REQ request. It is expected behavior.  

 

3.For the event of watchdog error, can customer check below register value to see whether the RSTB is asserted due to the Fault Error Counter intermediate value. 

diazmarin09_0-1697821544048.png

 

Regards,

David 

0 件の賞賛
返信

4,965件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello jvs0473,

I am pleased to contact you again.

I want you to know that we are working internally on your requested.

We will do our best to get back to you as soon as possible with a resolution to your issue.

I will appreciate your patience and  your understanding.

Regards,

David

0 件の賞賛
返信