bitbake stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake stuck

1,972 Views
Abhiram_m_s
Contributor I

Hello,
I am trying to build ros-image-core, but when i bitbake it, the server is stuck at 55%. i am using ubuntu 20.04 and trying to build bsp version 40.0.
Please let me know how to resolve the issue.

Thank you.
Regards.
Abhiram M S

0 Kudos
Reply
3 Replies

1,925 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback.

1. source ./nxp-setup-alb.sh -m s32g399ardb3ubuntu

2. bitbake fsl-image-ubuntu-ros

Best Regards

Chenyin

 

0 Kudos
Reply

1,937 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the questions

From the BSP40.0 UM, the only images that related with ROS is fsl-image-ubuntu-ros,  have you ever tried it before?

 

Best Regards

Chenyin

0 Kudos
Reply

1,934 Views
Abhiram_m_s
Contributor I

when i try to run fsl-image-ubuntu-ros, i am getting "Machine not supported error". I am using S32G399ARDB3 board. How do i proceed?

0 Kudos
Reply