Why did they use the different function interface to initialize platform on s32g3 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why did they use the different function interface to initialize platform on s32g3 ?

Jump to solution
5,241 Views
fengxianeric
Contributor III

Hi, I am planning to integrate ipcf single instance code from SW32G_IPCF_4.8.0_D2212 and llce sample code from Can_Llce_DS_Can2Can_S32G399A_M7, and they use the different calling method althogh they used the same rtd version (4.0.0), what's the reason ? 

PlatformInit(); // llce sample main

Platform_Init(NULL_PTR);  // ipcf instance main
 

plz discuss on how to use platform initialization function when they work together ?  thanks.

 

0 Kudos
Reply
1 Solution
5,132 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We don't understand the following comment:

"Plus tesing, the commented code snippets within

PlatformInit(void) 

which will make serial terminal failed to work,"

We don't the see usage of a serial terminal on both programs, which we do not understand.

Also, if you comment them they will make it work? Or if you comment them it will fail?

Please, let us know.

View solution in original post

0 Kudos
Reply
9 Replies
5,232 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Even though you are seeing that LLCE and IPCF example may have a different init function, under the LLCE example it can be seen that the "PlatformInit()" function referenced under the main function redirects to the "Platform_Init(NULL_PTR)" you are seeing at the IPCF example.

At the end, both example uses the same "Platform_Init(NULL_PTR)" function you are saying.

Please, let us know.

0 Kudos
Reply
5,221 Views
fengxianeric
Contributor III

Thanks caring,  tested today with such code altered,

int main(void)
{
   // PlatformInit();
Platform_Init(NULL_PTR);  // eric
    
    Llce_Firmware_Load();
    Can_Driver_Sample_Test();
 
  //  while (1);
    vTaskDelay(500);
 
    Can_Driver_Sample_Test();
    vTaskDelay(500);
 
       while (1)   {
          Can_Driver_Sample_Test();
 
            vTaskDelay(500);
       }
 
}
 
As a result, I failed to snap frame out, but I can detected frames if switching back to PlatformInit(), thanks.
0 Kudos
Reply
5,178 Views
fengxianeric
Contributor III

Thanks caring, initially tested below combinations,

only Platform_Init(NULL_PTR);    ----->  ipcf works, no work for llce

only PlatformInit(); ------> uboot cmd shell chaos/mixed after startm7

both --------> same phenomenon with PlatformInit()

And then do you have smart idea to correct my code ?

Thanks again

0 Kudos
Reply
5,202 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The behavior you are seeing is correct, since "PlatformInit()" function contains much more than only the "Platform_Init(NULL_PTR)". What we were referring in our previous comment was that it also contained the function used under the IPCF example, but not that it was the only one.

Please, let us know.

0 Kudos
Reply
5,160 Views
fengxianeric
Contributor III

Hello, again update testing today,  I commented all functions before Platform_Init, problems come out when I comment second function with PlatformInit(),

void PlatformInit(void)
{
    /* Configure S32G clocks */
    /* Enable LLCE partition */
    Mcu_Init(MCU_VARIANT);
    Mcu_InitClock(McuClockSettingConfig_0);  //  problem coming
//     while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() )
//     {
//         /* Busy wait until the System PLL is locked */
//     }
//     Mcu_DistributePllClock();
//     Mcu_SetMode(McuModeSettingConf_0);

// #ifdef USE_PORT_HLD
//     Port_Init(PORT_VARIANT);
// #else
//     Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
// #endif

//     OsIf_Init(NULL); /* enable system timer for timeout detection */

    /* Configurations for IRQ routing, priority and enable through Platform plugin. */
    Platform_Init(NULL);

    // Can_Enable_Timestamp();

}
 
THanks
0 Kudos
Reply
5,143 Views
fengxianeric
Contributor III

Plus tesing, the commented code snippets within

PlatformInit(void) 

which will make serial terminal failed to work,

 /* Configure S32G clocks */
    /* Enable LLCE partition */
    Mcu_Init(MCU_VARIANT);
    ///////////////////////////////////////////////////////

    // Mcu_InitClock(McuClockSettingConfig_0);  //  problem coming
    // while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() )
    // {
    //     /* Busy wait until the System PLL is locked */
    // }
   
    //  Mcu_DistributePllClock();
    // Mcu_SetMode(McuModeSettingConf_0);
//////////////////////////////////////////////////////////////////////
0 Kudos
Reply
5,133 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We don't understand the following comment:

"Plus tesing, the commented code snippets within

PlatformInit(void) 

which will make serial terminal failed to work,"

We don't the see usage of a serial terminal on both programs, which we do not understand.

Also, if you comment them they will make it work? Or if you comment them it will fail?

Please, let us know.

0 Kudos
Reply
5,014 Views
fengxianeric
Contributor III
Plz permit me to add comments in detail based on your response,
We don't understand the following comment:

"Plus tesing, the commented code snippets within
PlatformInit(void)
which will make serial terminal failed to work,"

We don't the see usage of a serial terminal on both programs, which we do not understand.
[explain] we make it run by uboot startm7 command.
Also, if you comment them they will make it work? Or if you comment them it will fail?
[explain] ipcf can work, but failed to run if we call this func within PlatformInit(void),
-----
Mcu_InitClock(McuClockSettingConfig_0); // problem coming
-----
it will make serial terminal "zombie", so I can't continue to run startm7 command ?
Clear now ?
THanks and sorry if giving not detailed description.
0 Kudos
Reply
5,102 Views
fengxianeric
Contributor III

Ipcf sample running by uboot command, I am doing integration with llce sample.

0 Kudos
Reply