Hi NXP Community,
I downloaded the "PFE-FW_S32G_1.5.0.zip".
According to "S32G2_LinuxBSP_32.0_User_Manual-1.pdf", I put "s32g_pfe_class.fw" & "s32g_pfe_util.fw" in some where, and modify the conf/local.conf.
But I got the debug message after boot:
[ 4.300371] pfeng 46000000.pfe: Firmware .elf detected [ 4.300374] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready. [ 4.300379] pfeng 46000000.pfe: Uploading CLASS firmware [ 4.300385] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready. [ 4.300389] pfeng 46000000.pfe: Selected FW loading OPs to load 8 PEs in parallel [ 4.320858] pfeng 46000000.pfe: Unsupported firmware detected: Found revision 1.5.0 (fwAPI:92367c0e25f21f49217a9b08168ad2c8), required fwAPI e1cb376b67fa4d1de800b132b328b42c [ 4.320886] pfeng 46000000.pfe: Classifier firmware loading the PE failed: 22 [ 4.320894] pfeng 46000000.pfe: Error during upload of CLASS firmware: 22 [ 4.321059] pfeng 46000000.pfe: HIF3 not enabled, skipped [ 4.321067] pfeng 46000000.pfe: HIF2 not enabled, skipped [ 4.321072] pfeng 46000000.pfe: HIF1 not enabled, skipped [ 4.321079] pfeng 46000000.pfe: HIF0 not enabled, skipped [ 4.321530] pfeng: probe of 46000000.pfe failed with error 5 |
I think I downloaded the wrong PFE firmware.
Which version of PFE firmware should I use?
已解决! 转到解答。
Hi,
Under the BSP33.0 Release notes, the compatible FW versions are provided. The following image is shown in the document:
Which indeed shows that PFE FW 1.3.0 is the one compatible with BSP33.0.
Please, let us know.
Hi NXP Community,
As the log:
[ 4.320858] pfeng 46000000.pfe: Unsupported firmware detected: Found revision 1.5.0 (fwAPI:92367c0e25f21f49217a9b08168ad2c8), required fwAPI e1cb376b67fa4d1de800b132b328b42c |
I check the "PFE-FW_S32G_1.5.0_ReleaseNotes.pdf":
The correct PFE firmware version for me is 1.3.0.
Am I right?
Hi,
Under the BSP33.0 Release notes, the compatible FW versions are provided. The following image is shown in the document:
Which indeed shows that PFE FW 1.3.0 is the one compatible with BSP33.0.
Please, let us know.