Whether the IPCF user space code supports multiple instances?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether the IPCF user space code supports multiple instances?

1,063件の閲覧回数
jiahaisheng
Contributor I

Hi Team,

    Does the IPCF user state code support multiple instances?

    I see finit_module in the os_init function, and as far as I know, each ipc-shm-uio.ko only allows finit_module once.

    Looking forward to reply!

0 件の賞賛
返信
1 返信

1,053件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We may not be understanding the overall request, if so we apologize.

Under the AN13750 available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors) a multi-instance IPCF application is implemented, where 3 M7 cores and the A53 cluster are used. Since the A53 is running linux, we suppose that it supports the multi-instance application.

For BSP33.0 (which is the ones being used under the AN) there is a required patch for IPCF multi-instance, which is also provided under the AN13750SW package under the S32G2 product page.

Please, let us know.

0 件の賞賛
返信