The command of receive CAN message

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The command of receive CAN message

397 次查看
Wzlinux
Contributor III

HI dear.

I am using S32G3 board doing the CAN message testing. 

after the config, I can use cansend command send the  CAN messages. 

And i want to receive CAN message from the PC. 

Does the BSP has receive command of CAN message?

Wzlinux_0-1739443037705.png

Wzlinux_1-1739443109462.png

 

标记 (1)
0 项奖励
回复
1 回复

392 次查看
Joey_z
NXP Employee
NXP Employee

Hi,Wzlinux

Thank you for contacting us.

Do you want to test receive command in the BSP? You can refer to the LinuxBSP_xx_User_Manual.pdf as shown in the following picture.

Joey_z_0-1739444486532.png

BR

Joey

0 项奖励
回复