The command of receive CAN message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The command of receive CAN message

462件の閲覧回数
Wzlinux
Contributor III

HI dear.

I am using S32G3 board doing the CAN message testing. 

after the config, I can use cansend command send the  CAN messages. 

And i want to receive CAN message from the PC. 

Does the BSP has receive command of CAN message?

Wzlinux_0-1739443037705.png

Wzlinux_1-1739443109462.png

 

タグ(1)
0 件の賞賛
返信
1 返信

457件の閲覧回数
Joey_z
NXP Employee
NXP Employee

Hi,Wzlinux

Thank you for contacting us.

Do you want to test receive command in the BSP? You can refer to the LinuxBSP_xx_User_Manual.pdf as shown in the following picture.

Joey_z_0-1739444486532.png

BR

Joey

0 件の賞賛
返信