SD on S32g rdb2 cannot generate insertion and remove interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD on S32g rdb2 cannot generate insertion and remove interrupt

ソリューションへジャンプ
2,666件の閲覧回数
HangSong
Contributor II

Hi @nxp,

Can't S32G RDB2 perform SD card plug-in detection through CD?

I am doing SD card support on S32G RDB2.
IRQSTATEN and IRQSIGEN write 0x17f00c3, enabling CINSSEN and CRMSEN.
When the SD card is pulled out and inserted, there will be no corresponding interrupt, and the register PRSSTAT[CINST], INT_STATUS[CINS] and INT_STATUS[CRM] will not change.

Thanks,
Song

タグ(2)
0 件の賞賛
返信
1 解決策
2,631件の閲覧回数
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,632件の閲覧回数
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

0 件の賞賛
返信
2,617件の閲覧回数
HangSong
Contributor II

Hi @bpe ,

Got it. Thank you.

Best Regards,
Song

 

0 件の賞賛
返信