SD on S32g rdb2 cannot generate insertion and remove interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SD on S32g rdb2 cannot generate insertion and remove interrupt

跳至解决方案
2,687 次查看
HangSong
Contributor II

Hi @nxp,

Can't S32G RDB2 perform SD card plug-in detection through CD?

I am doing SD card support on S32G RDB2.
IRQSTATEN and IRQSIGEN write 0x17f00c3, enabling CINSSEN and CRMSEN.
When the SD card is pulled out and inserted, there will be no corresponding interrupt, and the register PRSSTAT[CINST], INT_STATUS[CINS] and INT_STATUS[CRM] will not change.

Thanks,
Song

标记 (2)
0 项奖励
回复
1 解答
2,652 次查看
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,653 次查看
bpe
NXP Employee
NXP Employee

uSDHC SD Card detect signals are not routed outside S32G2, this function is not
available on it.

Best Regards,
Platon

 

0 项奖励
回复
2,638 次查看
HangSong
Contributor II

Hi @bpe ,

Got it. Thank you.

Best Regards,
Song

 

0 项奖励
回复