S32g2 LLCE range Filter Usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32g2 LLCE range Filter Usage

Jump to solution
2,001 Views
youke
Contributor III

hi nxp,

I am using the S32G2 development board to test the functionality of llce, and I have found that the range filter cannot be configured in EB. How can I configure it?
As shown in the figure below, it is not selectable in my EB

youke_0-1735261368877.png

My LLCE version is: S32G_LLCE_1_0_8

 

Tags (2)
0 Kudos
Reply
1 Solution
1,985 Views
Joey_z
NXP Employee
NXP Employee

hi,youke

You need to enable the container.

Joey_z_0-1735267104065.png

BR

Joey

 

View solution in original post

0 Kudos
Reply
3 Replies
1,985 Views
Joey_z
NXP Employee
NXP Employee

hi,youke

You need to enable the container.

Joey_z_0-1735267104065.png

BR

Joey

 

0 Kudos
Reply
1,982 Views
youke
Contributor III

hi joey,

Thank you, as I am a novice at EB, I asked this simple question;
Thank you for your support

0 Kudos
Reply
1,985 Views
youke
Contributor III

hi nxp,

I checked the source code Can_43_LLCE.xdm of EB and found that the RangeFilter value is false. After manually changing it to true, the range in EB can be configured,
I don't think manually modifying XDM is correct. How should I proceed correctly?

youke_0-1735266607881.png

 

0 Kudos
Reply