S32g SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32g SDK

3,349件の閲覧回数
rw1
Contributor I

Hello, I installed the S32 Studio with the S32G development package extension.

I can now create a project with the compiler we're using.

 

But if I open the "Config Tools Overview", the tool is telling me that there is no configuration created yet.

How can I create this configuration?

As I created the project, I could also not select the SDK to be used. Maybe this is the problem but I also could not find where to download an SDK for the S32G.

 

I basicly just want to use the S32 Studio to create our DCD configuration.

 

Thank you.

0 件の賞賛
返信
6 返答(返信)

3,324件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Roman Wenzler

 

Hope you are doing well

I think you have not created configuration. do as below after creation application project.

i.e I have created application project name as "MyTest"

 

Select the project in Project Explorer bar shown as below

Screenshot-1.png

 

Now Select DCD tool shown as below

Screenshot-3.png

 

Now Select the project as shown below

Screenshot-4.png

 

Now DCD confrontation will open as below. you can config DCD here

Screenshot-5.png

 

Now open Config Tools Overview you will see  as below

Screenshot-6.png

 

Hope this will help you,

 

Regards ,

Tushar

0 件の賞賛
返信

3,316件の閲覧回数
rw1
Contributor I

Hello and thank you for the fast response.

Unfortunately I can select my test project in the DCD view but it will not be locked in by the tool. The menu jumps back to <Select Project>.

 

I don't know if this may be part of the problem, but there are no SDKs to select when I go to my project properties and then "SDK".

 

Thank you.

0 件の賞賛
返信

3,307件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Roman Wenzler

 

Did you installed RTD ? if not , you can download from flexera and install.

can you please check SDKs window as below , i have RTD 3.0.2 , RTD 3.0.3 ,RTD  4.0.1 installed in my pc as

shot.png

 

0 件の賞賛
返信

3,301件の閲覧回数
rw1
Contributor I

Hello again,

as I stated in my first reply, I got no proper SKDs installed.

I only find SDKs for S32K and S32V but none for S32G.

Can you provide a download link for that?

 

Thank you.

0 件の賞賛
返信

3,149件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Roman Wenzler

 

Sorry for late reply as i was on leave. I conformed with our internal team , There isn't a separate software package called SDK of S32G, but the S32 Real-Time Drivers(RTD) contains S32G development package. install RTD package for same. can you check by installing it. let us know if more quarry

 

Regards ,

Tushar

0 件の賞賛
返信

3,264件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi

To Config DCD there are no requirement of SDK. we recommend of to install RTD. i have asked about this to our internal team for conformation of SDK. i will update here as soon as possible here about SDK

0 件の賞賛
返信