Hello, I installed the S32 Studio with the S32G development package extension.
I can now create a project with the compiler we're using.
But if I open the "Config Tools Overview", the tool is telling me that there is no configuration created yet.
How can I create this configuration?
As I created the project, I could also not select the SDK to be used. Maybe this is the problem but I also could not find where to download an SDK for the S32G.
I basicly just want to use the S32 Studio to create our DCD configuration.
Thank you.
Hi Roman Wenzler
Hope you are doing well
I think you have not created configuration. do as below after creation application project.
i.e I have created application project name as "MyTest"
Select the project in Project Explorer bar shown as below
Now Select DCD tool shown as below
Now Select the project as shown below
Now DCD confrontation will open as below. you can config DCD here
Now open Config Tools Overview you will see as below
Hope this will help you,
Regards ,
Tushar
Hello and thank you for the fast response.
Unfortunately I can select my test project in the DCD view but it will not be locked in by the tool. The menu jumps back to <Select Project>.
I don't know if this may be part of the problem, but there are no SDKs to select when I go to my project properties and then "SDK".
Thank you.
Hi Roman Wenzler
Did you installed RTD ? if not , you can download from flexera and install.
can you please check SDKs window as below , i have RTD 3.0.2 , RTD 3.0.3 ,RTD 4.0.1 installed in my pc as
Hi Roman Wenzler
Sorry for late reply as i was on leave. I conformed with our internal team , There isn't a separate software package called SDK of S32G, but the S32 Real-Time Drivers(RTD) contains S32G development package. install RTD package for same. can you check by installing it. let us know if more quarry
Regards ,
Tushar
Hi
To Config DCD there are no requirement of SDK. we recommend of to install RTD. i have asked about this to our internal team for conformation of SDK. i will update here as soon as possible here about SDK