S32G3 serial RCON

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 serial RCON

Jump to solution
1,364 Views
XD
Contributor II

Hi,

I am reviewing the serial RCON configuration. In the RMS32G3 manual, section 31.3.2.3, it mentions using RCON[7:8] to connect to the EEPROM. However, in AN13456 (S32G3 Boot Process), section 5.4, it states that the BootROM assumes the EEPROM is connected to RCON8 and RCON9. Could you please clarify this discrepancy?

Thanks,

XD

0 Kudos
Reply
1 Solution
1,350 Views
Celeste_Liu
NXP Employee
NXP Employee

Dear @XD ,

Thanks for contacting NXP support. After reviewing the information, we confirm that you should follow the instructions in the RMS32G3 manual. The configuration mentioned in that manual is the correct one for your reference.
If you have any further questions, please don't hesitate to contact us.
Best regards,

Celeste

View solution in original post

0 Kudos
Reply
1 Reply
1,351 Views
Celeste_Liu
NXP Employee
NXP Employee

Dear @XD ,

Thanks for contacting NXP support. After reviewing the information, we confirm that you should follow the instructions in the RMS32G3 manual. The configuration mentioned in that manual is the correct one for your reference.
If you have any further questions, please don't hesitate to contact us.
Best regards,

Celeste

0 Kudos
Reply