S32G3 goldbox M& TCPIP LWIP example does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 goldbox M& TCPIP LWIP example does not work

2,515 Views
rizwan_at_disruptdotcom
Contributor III

SDK version:
S32 Real-Time Drivers Version 5.0.0 QLP03
TCPIP_STACK for S32G version 2.0.0

Tool version:
S32 Design Studio for S32 Platform

Version: 3.6.4

Build id: 250929


Example:
lwip_FreeRTOS_S32G399A_M7_group lwIP TCP/IP stack
Basic application that presents the lwIP usage with S32G399A RTD

Summary of issue:
The example was built and flashed to QSPI NOR flash using the S32 Flash tool.
But GMAC ping does not work as laptop on the other end never detects the link.
the lights on GMAC are always on which also does not look right.


20251202_142757.jpg

Need help to be able to test the LWIP demo with FreeRTOS.

Labels (1)
0 Kudos
Reply
4 Replies

2,179 Views
rizwan_at_disruptdotcom
Contributor III

I have also tried the baremetal example for LWIP. The ccs: Bus error does not appear but still no ping response. I see that there are some tx interrupts initially for ARP tx, but i dont see any frames on ethernet where I have test laptop doing a tcpdump. The interface on laptop is also configured on the right subnet with sudo addr add 192.168.0.10/24 since lwip example takes 192.168.0.200 IP address. We need to be able to run LWIP stack so that we can develop on top of it. For this we need a working LWIP example for S32G3. We would really appreciate some support here.

0 Kudos
Reply

2,490 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @rizwan_at_disruptdotcom 

Thanks for your post.

According to the corresponding document, it is suggested using the following RTD/FreeRTOS packages listed:

chenyin_h_0-1764734340981.png

Would you mind retesting it with the recommended version?

 

BR

Chenyin

0 Kudos
Reply

2,245 Views
rizwan_at_disruptdotcom
Contributor III

@chenyin_h 

I have the same versions:

rizwan_at_disruptdotcom_0-1765444384439.png

 



When I step over device_init() I also see:

gta is listening on port 45000.

ccs:Bus error

ccs:Bus error

ccs:Bus error

ccs:Bus error

ccs:Bus error

ccs:Bus error

I am stuck on this problem for over a week now. Can you please provide a concrete working example that runs out of the box for S32G3 golbox rdb3?
Or maybe help me debug the problem?

0 Kudos
Reply

2,240 Views
rizwan_at_disruptdotcom
Contributor III

@chenyin_h 

I also found this in the release notes:

rizwan_at_disruptdotcom_0-1765446380220.png

 

Does this mean it may not work for S32G399A with Goldbox RDB3? In that case, any idea where can i get a working example for LWIP for S32G399A goldbox?

 

0 Kudos
Reply