S32G3 Internal RTC as WKUP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G3 Internal RTC as WKUP

ソリューションへジャンプ
1,943件の閲覧回数
wjb
Contributor I

Do you have a similar example as: "S32K344_Standby_RTC_Wakeup_Example"  for s32g3, using the internal RTC as wakeup source?

I am using board S32G-VNP-RDB3.

Thank you. -w

0 件の賞賛
返信
1 解決策
1,911件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,912件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

0 件の賞賛
返信