S32G3 Internal RTC as WKUP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G3 Internal RTC as WKUP

Jump to solution
1,948 Views
wjb
Contributor I

Do you have a similar example as: "S32K344_Standby_RTC_Wakeup_Example"  for s32g3, using the internal RTC as wakeup source?

I am using board S32G-VNP-RDB3.

Thank you. -w

0 Kudos
Reply
1 Solution
1,916 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

View solution in original post

0 Kudos
Reply
1 Reply
1,917 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The available example for RTC as wakeup source is provided under Linux itself, which is run under the A53 core.

Are you looking for an M7 example?

Please, let us know.

0 Kudos
Reply