S32G274a - eMMC boot blocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G274a - eMMC boot blocks

1,903 Views
nakrachi
Contributor II

Hello,

I am trying to boot from eMMC boot blocks BOOT0/1 partition (mmcblk0boot0 and mmcblk0boot1)

I loaded fip image at an offset of 0x1000, in both BOOT0/1 and User partitions.

I also updated PARTITION_CONFIG  to set it to boot from BOOT0 or BOOT1 partition, but no matter what I do, it always boots from USER partition.

I am wondering, if it is even possible to select boot partitions for booting ? is it a limitation of the BootROM ?

I've tried to set the boot partition with both Linux and u-boot, but no success so far.

=> mmc partconf 0
EXT_CSD[179], PARTITION_CONFIG:
BOOT_ACK: 0x1
BOOT_PARTITION_ENABLE: 0x1
PARTITION_ACCESS: 0x0

 

0 Kudos
Reply
3 Replies

1,858 Views
nakrachi
Contributor II

Thank you,

is there a workaround for this ? can the BootROM be updated/patched ?

0 Kudos
Reply

1,843 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. On regards of BootROM, we understand that there is no current patch (nor way to do it), we do apologize.

Please, let us know.

1,873 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi 

Overall, we understand that BootROM doesn’t support booting from boot partition of eMMC. We do apologize.

Please, let us know.

0 Kudos
Reply